The N7625C Signal Studio Pro for LTE/LTE-Advanced TDD 2026 software enables you to import waveforms to evaluate multi-standard radio (MSR) effects on LTE/LTE-Advanced TDD signals.
Below is a list of the Signal Studio waveforms that can be imported into the MSR feature for LTE/LTE-Advanced TDD signals.
N7600C Signal Studio for W-CDMA/HSPA+
N7601C Signal Studio for cdma2000/1xEV-DO
N7602C Signal Studio for GSM/EDGE/Evo
N7612C Signal Studio for TD-SCDMA/HSDPA
N7617C Signal Studio for WLANa
N7624C Signal Studio for LTE/LTE-Advanced FDD (non-MSR waveforms)b
N7625C Signal Studio for LTE/LTE-Advanced TDD (non-MSR waveforms)b
N7626C Signal Studio for V2X (non-MSR waveforms)b
N7631C Signal Studio for 5G NR
Supports high-resolution waveform export, providing better signal quality in the resulting MSR waveform.
Supports high-resolution waveform import and export, providing better signal quality in the resulting MSR waveform.
You cannot recursively import waveforms. That is, an MSR waveform cannot be used as a component waveform in a new MSR waveform. In this case, an error message appears in the status area.
In the figure below, an Library Waveform is selected for configuration. Refer to MSR: Generating a Library Waveform.
|
Carrier n -- Library Waveform |
|---|
MSR: Generating a Library Waveform
MSR: Using the Waveform Library Manager
Overcoming Test Challenges of MSR Base Station Components and Transmitters